-Xno_warning


This option suppresses outputting warning messages of the specified number.

[Specification format]

-Xno_warning={num|num1-num2}[, {num|num1-num2}]...

 

-

Interpretation when omitted

All warning messages are output.

[Detailed description]

-

This option suppresses outputting warning messages of the specified number.

-

Specify the error numbers as num, num1, and num2.
If the error number that does not exist, it will be ignored.

-

An error will occur if num, num1, or num2 is omitted.

-

If num1-num2 is specified, it is assumed that error numbers within the range have been specified.

-

When this option is specified more than once, all specifications will be valid.

-

The error number specified by this option is the rightmost 5 digits of the 7-digit number following the "W".
See "10. MESSAGE" for error numbers.

-

A message whose type was changed to error level by the -change_message option cannot be controlled by this option.

-

The message numbers that can be controlled by this option are as follows:

-

W0520000 to W0559999 [V1.06.00 or earlier]

-

W0510000 to W0559999 [V1.07.00 or later]

[Example of use]

-

To suppress outputting warning message "W0520111" describe as:

>ccrh -Xno_warning=20111 -Xcommon=rh850 main.c