Indicate to the assembler the start of a code section.
[Syntax]
Symbol field
|
Mnemonic field
|
Operand field
|
Comment field
|
[section-name]
|
.cseg
|
[relocation-attribute]
|
[; comment]
|
[Function]
- | The .cseg directive indicates to the assembler the start of a code section. |
- | All instructions described following the .cseg directive belong to the code section until it comes across a section definition directives. |
[Use]
- | The .cseg directive is used to describe instructions, .db, .dw directives, etc. in the code section defined by the .cseg directive. |
- | Description of one functional unit such as a subroutine should be defined as a single code section. |
[Description]
- | The start address of a code section can be specified with the .org directive. |
- | A relocation attribute defines a range of location addresses for a code section. |
Table 5.8 | Relocation Attributes of .cseg |
|
|
|
|
|
|
TEXT
|
Allocates the program.
|
.text
|
2
|
|
PCTEXT
[V1.07.00 or later]
|
Allocates position-independent programs.
|
.pctext
|
2
|
|
ZCONST
|
This section is for constant (read-only) data. It allocates a memory range (up to 32 Kbytes, in the positive direction from r0), referenced with 1 instruction using r0 and 16-bit displacement.
|
.zconst
|
4
|
|
ZCONST23
|
This section is for constant (read-only) data. It allocates a memory range (up to 4 Mbytes, in the positive direction from r0), referenced with 1 instruction using r0 and 23-bit displacement.
|
.zconst23
|
4
|
|
CONST
|
This section is for constant (read-only) data. It allocates a memory range (up to 4 Gbytes, in the positive direction from r0), referenced with 2 instructions using r0 and 32-bit displacement.
|
.const
|
4
|
|
PCCONST16
[V1.07.00 or later]
|
This section is for position-independent constant data (read-only). It allocates a memory range (up to ±32 Kbytes from __pc_data) referenced with 1 instruction using 16-bit displacement from the __pc_data symbol.
|
.pcconst16
|
4
|
|
PCCONST23
[V1.07.00 or later]
|
This section is for position-independent constant data (read-only). It allocates a memory range (up to ±4 Mbytes from __pc_data) referenced with 1 instruction using 23-bit displacement from the __pc_data symbol.
|
.pcconst23
|
4
|
|
PCCONST32
[V1.07.00 or later]
|
This section is for position-independent constant data (read-only). It allocates a memory range referenced with 2 instructions using 32-bit displacement from the __pc_data symbol.
|
.pcconst32
|
4
|
- | An error will occur in any of the following cases. |
- | If TEXT is specified when the -pic option has been specified |
- | If PCTEXT is specified when the -pic option has not been specified |
- | If CONST, ZCONST, or ZCONST23 is specified when the -pirod option has been specified |
- | If PCCONST16, PCCONST23, or PCCONST32 is specified when the -pirod option has not been specified |
- | The allocation section of instructions or data when no symbol definition directive has been written is the ".text” section if the -pic option has not been specified and the ".pctext” section if the -pic option has been specified. |
- | By describing a section name in the symbol field of the .cseg directive, the code section can be named. If no section name is specified for a code section, the assembler will automatically give a default section name to the code section.
The default section names of the code sections are shown below. |
- | The default section names have the relocation attributes shown above. Giving them any other attributes is not possible. |
- | The following characters are usable in section names. |
- | Alphanumeric characters (0-9, a-z, A-Z) |
- | Special characters (@, _, .) |