Sine
[Classification]
Mathematical library
[Syntax]
#include <mathf.h>
float sinf(float x);
[Return value]
Returns the sine of x.
If inputting +∞, sinf returns a NaN and sets macro EDOM to global variable errno.
If the solution is a denormal number, sinf sets macro ERANGE to global variable errno.
[Description]
This function calculates the sine of x. Specify the angle in radian.