This option suppresses outputting warning messages of the specified number.
[Specification format]
-no_warning_num={num|num1-num2}[,{num|num1-num2}]...
|
- | Interpretation when omitted |
All warning messages are output.
[Detailed description]
- | This option suppresses outputting warning messages of the specified number. |
- | Specify the error numbers as num, num1, and num2.
If the error number that does not exist, it will be ignored. |
- | An error will occur if num, num1, or num2 is omitted. |
- | If num1-num2 is specified, it is assumed that error numbers within the range have been specified. |
- | If this option is specified more than once, all of the given specifications will be effective. |
- | The error number specified by this option is the rightmost 5 digits of the 7-digit number following the "W". |
- | This option does not control messages that have been changed to be conveyed as errors with the -change_message option. |
- | This option controls the following message numbers. |
- | W0510000 to W0529999 and W0550000 to W0559999 [V1.05 or earlier] |
- | W0510000 to W0559999 [V1.06 or later] |
[Example of use]
- | To suppress outputting warning message "W0511146" and "W0511147", describe as: |
>ccrl -no_warning_num=11146,11147 -cpu=S2 -dev=dr5f100pj.dvf main.c
|