|
-CFI_IGNORE_Module [Professional Edition only] [V1.06 or later] |
This option specifies object files to be exempted from the function list for use in detecting illegal indirect function calls.
This option specifies object files to be exempted from the function list for use in detecting illegal indirect function calls. |
If this option is specified more than once, the functions of all specified object files are exempted from the function list. |
When this option is used, the -CFI option must also be specified. If the -CFI option is not specified, an error will occur. |