The registers used for passing arguments are AX, BC, and DE.
The targets for allocating arguments, argument types, and how to change the size are shown below.
Changes can be accepted only for those described below.
For the variable size or default argument promotions, see "(7) Default argument promotions". |
The argument immediately before a variable argument is handled as "when the function prototype can be referenced and the parameter type can be referenced". |
Arguments are allocated to registers as follows.
A target to be allocated to registers is an argument whose size is 4 bytes or less. |
When the argument is a structure or union, all members are allocated either to registers or in the stack. |
For a far pointer, the lower three bytes are allocated to registers. |
Register allocation is processed in the order from the first argument to the last argument (from left to right in the source program), and allocates each argument to the register with the highest priority among available registers. If there are no available registers, arguments are allocated in the stack. The priorities of the registers are shown below. |
|
Priority of Register to which Argument is Allocated (left side has the highest priority) |
|
"-" in this table is a symbol to associate 8-bit or 16-bit registers to other 16-bit registers.
Each argument is allocated to registers so that the descending order of addresses (from upper address to lower address) for the bytes composing the argument matches the register specification order (from left to right) shown in the above table.
When calling to a function declared as "void foo (char p1, short p2, char p3)", p1 is allocated to register A, p2 is allocated to register BC, and p3 is allocated to register X. |
When structure-type argument S shown below is allocated to registers, c1 is allocated to register X and s2 is allocated to register BC. Padding is allocated to register A. |
When calling to a function declared as "void foo (long x)", the upper 2 bytes of x are allocated to register BC and the lower 2 bytes are allocated to register AX. |
When structure-type argument S3 shown below is allocated to registers, the highest byte is allocated to register C, the next one byte is allocated to register A, and the lowest byte is allocated to register X. |
8-byte data, such as long long type data or double type data in the program to which option -dbl_size=8 is specified, is allocated in the stack |
A structure or union of five bytes or more is allocated in the stack while a structure or union of 4 bytes or less is a target for being allocated to registers. |
Arguments are allocated in the stack as follows.
Arguments to be passed by the stack are allocated in little endian mode and aligned at the 2-byte boundary. |
The order for allocating the arguments to be passed by the stack is that the more the argument is on the left side in the argument sequence, the address is smaller. |
The arguments to be passed by the stack are sequentially allocated in the stack except for the 1-byte padding which can be inserted between arguments. |
Each argument is allocated in the stack so that the descending order of addresses (from upper address to lower address) for the bytes composing the argument matches the descending order of addresses (from upper address to lower address) in the stack. |
For a far pointer, the lower three bytes are allocated to a 4-byte area in the stack. The value of the highest one byte of the 4 bytes is undefined. The page number part (= upper four bits of the 20-bit far address) of a far pointer is stored in the lower four bits of the second upper byte in the 4-byte area. |
For the method of stack allocation, see section "9.1.5 Stack frame". |
When calling to a function declared as "void foo (long long x)" and assuming that sp indicates the value of stack pointer immediately before the call site of the function, the highest one byte of x is allocated to the location indicated by sp + 7, each byte is allocated to sp + 6, sp + 5, sp + 4, sp + 3, sp + 2, and sp + 1 in the descending order of addresses, and the lowest byte is allocated to the location indicated by sp + 0. |