< Compile Options / Object Options >
When the stuff option is specified, all variables are allocated to 4-byte, 2-byte, or 1-byte boundary alignment sections depending on the alignment value (see table B-4). |
C, D, and B are the section names specified by the section option or #pragma section. W is the section name specified by the section option. The data contents allocated to each section are output in the order they were defined. |
.SECTION C_2,ROMDATA,ALIGN=2 .glb _c _c: .word 0000H .SECTION D_1,ROMDATA .glb _b _b: .byte 00H .SECTION B,DATA,ALIGN=4 .glb _a _a: .blkl 1 .SECTION B_1,DATA .glb _ST _ST .blkb 2 |