< Optimizing Linkage Editor (rlink) Options / Other Options >
The default for this option is memory = high.
When memory = low is specified, the linkage editor loads the information necessary for linkage in smaller units to reduce the memory occupancy. This increases file accesses and processing becomes slower when the occupied memory size is less than the available memory capacity. |
memory = low is effective when processing is slow because a large project is linked and the memory size occupied by the linkage editor exceeds the available memory in the machine used. |
compress, delete, rename, map, stack, cpu=stride, or
list and show[={reference | xreference}] are specified in combination.
delete, rename, extract, hide, or replace