|
RTSD
|
Releasing stack frame and returning from subroutine
|
RTSD
|
|
ReTurn from Subroutine and Deallocate stack frame
|
[Syntax]
(1)RTSD src
(2)RTSD src, dest-dest2
[Operation]
(1)SP = SP + src;
PC = *SP;
SP = SP + 4;
(2)signed char i;
SP = SP + ( src - ( register_num(dest2) - register_num(dest) +1 ) * 4 );
for ( i = register_num(dest); i <= register_num(dest2); i++ ) {
tmp = *SP;
SP = SP + 4;
register(i) = tmp;
}
PC = *SP;
SP = SP + 4;
[Function]
- | This instruction rotates dest one bit to the right including the C flag. |
- | This instruction restores values for the block of registers in the range specified by dest and dest2 from the stack. |
- | The range is specified by first and last register numbers. Note that the condition (first register number ? last register number) must be satisfied. |
- | The stack pointer in use is specified by the U bit in the PSW. |
- | Registers are restored from the stack from R1 to R15: |
[Instruction Format]
|
|
|
|
|
|
|
(1)RTSD src
|
#UIMM:8
|
–
|
–
|
|
|
(2)RTSD src, dest-dest2
|
#UIMM:8
|
Rd (Rd=R1~R15)
|
Rd2 (Rd=R1~R15)
|
|
[Flag Change]
- | This instruction does not affect the states of flags. |
[Description Example]
RTSD #4
RTSD #16, R5-R7