Defines the value to be set in errno when an error is generated in a library function.
The following macro names are all implementation-defined.
|
int type variable. An error number is set when an error is generated in a library function. |
||
|
Refer to section 10.5.6, Standard Library Error Messages. |
||