Renesas Electronics
top
Debug Tool
FUNCTIONS
Connect to/Disconnect from the Debug Tool
2.4
Connect to/Disconnect from the Debug Tool
This section describes how to connect to/disconnect from the debug tool.
Differences Information
Previous Topic
[Hook Transaction Settings] tab
Next Topic
Connect to the debug tool
Table of Contents
Overview
Preparation before Debugging
Configuration of Operating Environment of the Debug Tool
Connect to/Disconnect from the Debug Tool
Connect to the debug tool
Disconnect from the debug tool
Connect to the debug tool using hot plug-in [E1][E20]
Download/Upload Programs
Display/Change Programs
Usage of PIC/PID Function
Select a Core (PE)
Execute Programs
Stop Programs (Break)
Display/Change the Memory, Register and Variable
Display Information on Function Call from Stack
Collect Execution History of Programs
Measure Execution Time of Programs
Measure Performance [Full-spec emulator][E1][E20]
Measure Coverage [Simulator]
Set an Action into Programs
Manage Events
Use Hook Function
About Input Value
Exclusive Control Checking Tool
Pseudo-error Debugging [Full-spec emulator][E1][E20]
Debugging CAN Bus Reception Procedures [Full-spec emulator][E1][E20]
Measuring CAN Bus Reception Processing Times [E2]