2.13.6.2
Change display format of values
The display format of the [Line Number/Address], [Address] and [Data] area can be changed using buttons below on the toolbar.
Note that these buttons are disabled while the tracer is running.
|
Notation
|
The following buttons to change the notation of a data value are displayed.
|
|
|
Hexadecimal
|
Displays values on this panel in hexadecimal number (default).
|
|
Decimal
|
Displays values on this panel in decimal number.
|
|
Octal
|
Displays values on this panel in octal number.
|
|
Binary
|
Displays values on this panel in binary number.
|