2.14.2.3 Edit a Timer Result event [Full-spec emulator][E1][E20]

Detailed information on a Timer Result event is edited in the Detailed Settings of Timer Measurement dialog box [Full-spec emulator][E1][E20]. This dialog box is opened by selecting the Timer Result event you desire to edit on the Events panel then selecting [Edit Condition...] from the context menu.

In the Detailed Settings of Timer Measurement dialog box [Full-spec emulator][E1][E20], the following can be specified as measurement items.

Only a single item can be measured, and the measurement result for only the selected item is displayed on the Events panel.

Measurement Item

Function

Total Count

Measures the total execution time of the specified section.

Max Count

Measures the maximum execution time of the specified section.

Min Count

Measures the minimum execution time of the specified section.

Pass Count

Measures the pass count of the specified section.

This cannot be measured when an end condition has not been set.