2.8.1 Switching between cores (PEs)

The core (PE) to be debugged can be selected in either of the following two ways.

(1)

Switching through the statusbar

Select a desired PE from the drop-down list (shown below) on the statusbar in the Main window.

Figure 2.84

Statusbar on Main Window

Caution

When the drop-down list used for switching between cores on the status bar is being displayed while the size of this window is maximized, part of the list is hidden behind the task bar and thus cannot be selected.
Set the task bar to "Hide automatically" or set the location of the task bar as [Right], [Left], or [Upper].

(2)

Switching through the Debug Manager panel

Select a desired PE on the Debug Manager panel that are opened by selecting [Debug Manager] from the [View] menu.

Figure 2.85

Debug Manager Panel