2.10.2 Stop the program manually

The program in execution is forcibly stopped by clicking the button on the debug toolbar (Forced break function).

Remark

In cases of failure to stop a program during execution, the following setting may be required to allow stopping execution of the program.
However, stopping a program while this setting is in place leads to a CPU reset.

-

The [Reset While Running] category on the [Debug Tool Settings] tab of the Property panel

[Use the force reset] property

[Yes]