2.5.2.2
Add download files (*.hex/*.mot/*.bin)
Follow the steps below to add download files other than the load module file format (Intel HEX file (*.hex), Motorola S-record file (*.mot), or binary file (*.bin)) in the Download Files dialog box.
(1) | Click the [Add] button |
When the [Add] button is clicked, a blank list item "-" is displayed in the last line of the [Download file list] area.
(2) | Property configuration of the download files to add |
Configure the download conditions for the download file to add in the [Download file property] area.
Configure each item displayed with the following condition. When the configuration is completed, the file name specified in this property is displayed in the blank list of the [Download file list] area.
|
File
|
Specify the download file (Intel HEX file (*.hex), Motorola S-record file (*.mot), or binary file (*.bin)) to download (up to 259 characters).
|
|
Default
|
Blank
|
|
Modifying
|
Directly enter from the keyboard, or specify with the Select Download File dialog box opened by clicking the [...] button.
|
|
Available values
|
See "Table 2.1 Downloadable File Formats".
|
|
File type
|
Select the type of the file to download.
Here, select a item other than [Load module file].
|
|
Default
|
Load module file
|
|
Modifying
|
Select from the drop-down list.
|
|
Available values
|
Load module file
|
Specifies a load module file.
|
|
Hex file
|
Specifies an Intel HEX file.
|
|
S record file
|
Specifies a Motorola S-record file.
|
|
Binary data file
|
Specifies an binary file.
|
|
Offset
|
Specify the offset from the address at which the file's download is to start.
Note that this item appears only when [File type] is set to [Hex file] or [S record file].
|
|
Default
|
0
|
|
Modifying
|
Directly enter from the keyboard.
|
|
Available values
|
0x0 to 0xFFFFFFFFFF in hexadecimal number
|
|
Start address
|
Specify the address at which to start the file's download.
Note that this item appears only when [File type] is set to [Binary file].
|
|
Default
|
0
|
|
Modifying
|
Directly enter from the keyboard.
|
|
Available values
|
0x0 to 0xFFFFFFFFFF in hexadecimal number
|
Remark | The settings of whether to download the object information or symbol information can be made only when the type of the file to download is load module files. |
(3) | Check the order of download |
The order of the download is the display order of the files displayed in the [Download file list] area.
If you want to change the order, use the [Up]/[Down] button.
Enable all the configuration in this dialog box and add a download file (the file name is displayed in the [Download] category on the [Download File Settings] tab of the Property panel).