2.11.3 Display/change the I/O register

Contents of the I/O register can be displayed and its values can be changed in the IOR panel below.

Select the [View] menu >> [IOR].

For details on the contents and function in each area, see the section for the IOR panel.

Figure 2.105

Display the Contents of I/O register (IOR Panel)

 

This section describes the following.

 

2.11.3.1 Search for an I/O register

2.11.3.2 Organize I/O registers

2.11.3.3 Change display format of values

2.11.3.4 Modify the I/O register contents

2.11.3.5 Display/modify the I/O register contents during program execution

2.11.3.6 Save the I/O register contents