2.7.2.1 Execute after resetting microcontroller (CPU)

Click the button on the debug toolbar.

Reset CPU and start execution of the program from the reset address.

When this operation is performed, the program continues to be executed until either of the following occurs:

-

The button has been clicked (see "2.8.2 Stop the program manually").

-

The PC has reached a breakpoint (see "2.8.3 Stop the program at the arbitrary position (breakpoint)").

-

Other break causes have occurred.

Remark

This operation is the same as when the button is clicked after clicking the button.