2.8.1 Configure the break function

Before the break function can be used, it is necessary to make settings relating to the operation of a break.

This break operation can be configured in the [Break] category on the [Debug Tool Settings] tab of the Property panel.

The setting method differs depending on the debug tool used.

 

2.8.1.1 [IECUBE]

2.8.1.2 [E1]/[E20]/[EZ Emulator]

2.8.1.3 [Simulator]