2.8.4.2 Edit a break event (execution type)

It is possible to edit a break event (execution type) you have set.

For details on how to do it, see "2.15.4.1 Edit execution-related events" or "2.15.4.3 Edit combination conditions of events [E1] [E20]".

Caution

This function applies to only a break event (execution type) whose type is Hardware Break or Combination Break [E1][E20].