2.17.4 Editing detailed settings of events

This section describes how to edit detailed settings of various events. For information on editing of timer measurement events, see "2.14.3.3 Editing a timer measurement event [E1] [E20] [EZ Emulator]". For information on editing of action events (Printf events and interrupt events), see "2.16 Set an Action into Programs".

 

2.17.4.1 Editing execution-related events

2.17.4.2 Editing access-related events

2.17.4.3 Editing combination conditions of events [E1] [E20] [EZ Emulator]