2.13.6.2 Changing the form in which values are displayed

The form in which values are displayed in the [Line Number/ Address], [Address], and [Data] areas can be freely changed by using the toolbar buttons shown below.

However, these buttons are disabled during program execution.

Notation

Shows the following buttons that change the form in which values are displayed.

 

 

Displays values on this panel in hexadecimal (default).

 

Displays values on this panel in decimal.

 

Displays values on this panel in octal.

 

Displays values on this panel in binary.