2.9.2.1 Execute after resetting microcontroller (CPU)

You can reset the CPU and start the execution of the program from the reset address.

Click the button on the debug toolbar.

When this operation is performed, the program continues to be executed until either of the following occurs:

 

-

The button has been clicked (see "2.10.1 Stop the program manually").

-

The PC has reached a breakpoint (see "2.10.2 Stop the program at the arbitrary position (breakpoint)").

-

Other break factors have occurred.

 

Remark

This operation is the same as when the button is clicked after clicking the button.