5.5 Warnings

Table 5.5

Warnings

W0023001

[Message]

No Tag 'xxx'.

W0023002

[Message]

Invalid data.

W0024001

[Message]

No Tag 'xxx'.

W0024002

[Message]

Invalid data.

W0130000

[Message]

Following updates are not displayed because the necessary license is not registered.

W0140018

[Message]

Installation succeeded.

To complete the installation, please reboot your computer.

[Explanation]

This appears when the entire installation was successful, and a restart is necessary.

W0140022

[Message]

The installation was interrupted before it finished.

[Explanation]

This appears when the installation is aborted before completion.

W0140025

[Message]

The installation was aborted before finish.

Please reboot your computer.

[Explanation]

This appears when the installation was aborted, and the installation of the completed portion (before cancelling) requires a restart.

W0140031

[Message]

To complete the uninstallation, it is necessary to reboot your computer.

W0140042

[Message]

The following products are required to reboot Windows to complete the installation.

Please reboot your computer.

- xxx

:

 

Please install the latest service packs and security updates for this product using Windows Update and Microsoft Update.

 

Stop the installation.

[Explanation]

This message appears when all installation of required environments has succeeded, and a reboot is required for all of them.

W0140043

[Message]

The following products are required to reboot Windows to complete the installation.

Please reboot your computer.

- xxx

:

 

The following product succeeded in installation.

- xxx

:

 

Please install the latest service packs and security updates for this product using Windows Update and Microsoft Update.

 

Stop the installation.

[Explanation]

This message appears when all installation of required environments has succeeded, and a reboot is required for some of them, but not for others.

W0190002

[Message]

Failed to read license information from "xxx". The file is broken.

W0190003

[Message]

Failure in reading license information. The file is corrupted.

W0200001

[Message]

There are multiple files used for inquiry and update in your PC. The file should be unique. Please reinstall xxx.

[Explanation]

This appears when there is more than one information files used to update and obtain information about the software.

Perform the installation again.

[Action by User]

Perform the installation again.

W0201003

[Message]

Could not Change the Writable.

[Explanation]

This message appears when can't change the " reading exclusive use" attribute of the target file.

[Action by User]

Specify the file by which the current user can edit the attribute.

W0201004

[Message]

Illegal extension of the file. The extension of xxx must be specified for the extension of the file.

[Explanation]

This appears when the extension of a file being loaded or imported is not supported.

[Action by User]

Specify a file with a correct extension.

W0201005

[Message]

Illegal encode of the file. The encode of xxx must be specified for the encode of the file.

[Explanation]

This appears when the encoding of a file being loaded or imported is not supported.

[Action by User]

Specify a correct file encoding.

W0202001

[Message]

Diverting the project failed. The file composition and the properties of the tool is not applied.

[Explanation]

This appears in cases such as when creating a new project using the copy project feature, and the project to copy could not be parsed. The properties of the file-hierarchy or tools could not be applied.

[Action by User]

Copy a file that can be parsed successfully.

W0202002

[Message]

Applying the properties of the tool failed. (Target tools: xxx)

[Explanation]

This appears in cases such as when creating a new project using the copy project feature, and a failure occurs while applying the tool properties. The file hierarchy of the copied project file has been applied.

[Action by User]

Copy a file that can be parsed successfully.

W0202003

[Message]

The project file can be restored. But if you save the project, some information may be lost.

[Explanation]

Tried to read the project file by which the compatibility isn't perfection. Can return, but when saved overwrite, a part of information is lost.

[Action by User]

Confirm whether it's identical with tool version made created project file. When it's necessary, update integrated development environment framework and a plug-in.

W0202004

[Message]

There is a plug-in that doesn't correspond to the version of the specified compiler package. See the [All Messages] tab in the Output panel.

[Explanation]

Some or all plug-ins no longer function because the compiler version has changed.

[Action by User]

Make sure that the versions of the plug-ins and compiler package are compatible.

W0202005

[Message]

Can not open the project with last saved status. See the [All Messages] tab in the Output panel.

[Explanation]

This appears when loading a project, and the project could not be loaded with the last status saved.

W0202006

[Message]

Can not import the project with last saved status. See the [All Messages] tab in the Output panel.

[Explanation]

This message appears if the project could not be imported with the last saved status when importing build options.

W0203001

[Message]

Enabled the feature of applying the setting value for a property to all build modes at once.

Please note that the setting value can be the incompatible value for other build mode.

[Explanation]

This message appears when the [Change property value for all build modes at once] property is set to [Yes].

W0205001

[Message]

Fewer than xxx or more than yyy characters cannot be specified.

[Explanation]

This message appears in the Message dialog box if a string is specified for the area that is shorter than xxx characters, or longer than yyy characters, when xxx and yyy are the minimum and maximum lengths, respectively.

The values of xxx and yyy are dependent on the input area.

[Action by User]

Specify a value that is in bounds.

W0205002

[Message]

More than xxx characters cannot be specified.

[Explanation]

This message appears when a line in the display source set in the Text Edit dialog box is longer than the maximum number of characters.

[Action by User]

Shorten the line that is greater than the maximum length so that it is within the maximum number of characters.

W0205003

[Message]

More than xxx lines cannot be specified.

[Explanation]

This message appears when the display source set in the Text Edit dialog box is longer than the maximum number of lines.

[Action by User]

Make sure that the number of lines is no more than the maximum limit.

W0205004

[Message]

Specify xxx digits in hexadecimal.

[Explanation]

This message appears when the string contains characters that cannot be used to represent a base-16 number, including when the number of digits is valid.

[Action by User]

Specify a hexadecimal number with effective number of digits.

W0205006

[Message]

Specify a numerical value.

[Explanation]

A number specifying an area includes non-numeric characters.

[Action by User]

Specify numeric characters.

W0205007

[Message]

Specify in decimal.

[Explanation]

A decimal number specifying an area includes characters that cannot be used to represent a decimal number.

[Action by User]

Specify numeric characters as base-10.

W0205008

[Message]

Fewer than xxx or more than yyy values cannot be specified.

[Explanation]

This message appears when an out-of-range value is entered into a number input area in the properties or the like.

[Action by User]

Specify a value between xxx and yyy.

W0205009

[Message]

Only ASCII character sets can be entered.

[Explanation]

Numeric or ASCII characters specifying an area include characters that are not numeric or ASCII.

[Action by User]

Specify a string that is a valid number or a valid ASCII string.

W0205010

[Message]

Specify a character string.

[Explanation]

The field is empty.

[Action by User]

Specify a valid string.

W0205011

[Message]

Specify a path.

[Explanation]

The field is empty.

[Action by User]

Specify a valid path.

W0205012

[Message]

The specified path contains a non-existent folder.

[Explanation]

The specified path includes a non-existent folder.

[Action by User]

Specify a valid path.

W0205013

[Message]

The file name or path name is invalid. The characters (* ? " < > | ) cannot be used.

[Explanation]

The string includes illegal characters.

[Action by User]

Specify a valid path.

W0205014

[Message]

The format is invalid.

[Explanation]

This message appears when a string with invalid format is entered into the properties or the like having a specific format.

[Action by User]

Enter a string in accordance with the specified format.

W0205015

[Message]

Specify in hexadecimal.

[Explanation]

A hexadecimal number specifying an area includes characters that cannot be used to represent a hexadecimal number.

[Action by User]

Specify numeric characters as base-16.

W0205016

[Message]

Specify in decimal or hexadecimal.

[Explanation]

A decimal/hexadecimal number specifying an area includes characters that cannot be used to represent a decimal/hexadecimal number.

[Action by User]

Specify a valid string of numeric characters in base-10 or base-16.

W0205017

[Message]

Enter a value smaller than the end address for the start address.

[Explanation]

This message appears when an area in which an address or symbol range is specified has a start address that is larger than the end address.

[Action by User]

Specify an end address that is larger than the start address.

W0205018

[Message]

Enter a value in the range of xxx to yyy.

[Explanation]

This message appears when an area in which an address or symbol range is specified has a value greater than the address space of the debugging tool.

[Action by User]

Specify an address range that fits in the address space of the debugging tool.

W0205020

[Message]

The address cannot be omitted.

[Explanation]

This message appears when an area for an address/symbol is left blank, and blank entries are not allowed.

[Action by User]

Specify an address, symbol, or address expression.

W0205021

[Message]

The character string is too long. Specify a character string with xxx or fewer characters.

[Explanation]

This message appears when a string was specified in a string area that was longer than the maximum length.

[Action by User]

Specify a string of no more than the maximum number of characters.

W0205022

[Message]

The address expression is invalid. Specify a symbol or numerical value.

[Explanation]

This message appears when a string that is invalid as an address expression is entered in an area for specifying an address expression.

[Action by User]

Specify a string that is correct as an address expression.

W0205023

[Message]

The specified value is out of range.

[Explanation]

This message appears when an out-of-bounds value is entered into a numeric input area in the properties or the like.

[Action by User]

Enter a value within the correct range.

W0205024

[Message]

The file name is invalid. The characters ( \\ / : * ? " < > | ) cannot be used.

[Explanation]

The string includes illegal characters.

[Action by User]

Specify a valid file name.

W0205025

[Message]

xxx cannot be specified.

[Explanation]

This message appears when an input value in the properties could not be specified especially.

[Action by User]

Specify the different value within the correct range.

W0205026

[Message]

Can not specify the odd address.

[Explanation]

This message appears when the value entered in the field for a property is odd but an even value is required.

[Action by User]

Specify an even value.

W0205027

[Message]

Names that begin with a number can not be specified.

[Explanation]

This message appears when no names that begin with numbers are allowed.

[Action by User]

Specify a name that does not begin with a number.

W0205028

[Message]

Can not specify a reserved word. (xxx)

[Explanation]

This message appears when the specified value is invalid as a reserved word. xxx indicates a list of reserved words.

[Action by User]

Specify a value that is not a reserved word.

W0208001

[Message]

Break could not be set. Specify a global variable.

[Explanation]

Failed to set a breakpoint that is triggered when a global variable is read, written, or read/written.

[Action by User]

Specify a global variable in the Editor panel or Watch panel.

W0208002

[Message]

Setting for recording to trace could not be done. Specify a global variable.

[Explanation]

Failed to set a trace that logs when a global variable is read, written, or read/written.

[Action by User]

Specify a global variable in the Editor panel or Watch panel.

W0208003

[Message]

Setting for recording to timer could not be done. Specify a global variable.

[Explanation]

Failed to configure timer control when a global variable is read, written, or read/written.

Specify a global variable in the Editor panel or Watch panel.

[Action by User]

Specify a global variable in the Editor panel or Watch panel.

W0209001

[Message]

Executing program ...

[Explanation]

The action cannot be performed because the program is running.

[Action by User]

Perform the action again after the program execution halts.

W0210001

[Message]

The connection to the debugger was completed, but the following problem may exist.

[Explanation]

Displays a warning to check the connection of the target card.

[Action by User]

Check the connection of the conversion adapter (EA).

We recommend attaching the conversion adapter when a target is not connected.

W0210002

[Message]

Download was completed, but the following problem may exist.

[Explanation]

A warning appears upon download.

W0210003

[Message]

Software break and hardware break are conflicted. Invalid instruction may be executed by restart.

[Explanation]

This appears when software breakpoint and hardware breakpoint are conflicted.

[Action by User]

The PC value may be invalid.

Reset CPU, and execute it again.

W0210004

[Message]

Some RAM or register values are not restored due to some kind of problem.

[Explanation]

This message appears when loading of RAM or register values has failed.

[Action by User]

(1)

Check the emulator power.

(2)

Check whether the USB cable isn't cut.

(3)

Follow the instructions in the message to remedy the problem.

W0210005

[Message]

Some RAM or register values are not saved due to some kind of problem.

[Explanation]

This message appears when saving of RAM or register values has failed.

[Action by User]

(1)

Check the emulator power.

(2)

Check whether the USB cable isn't cut.

(3)

Follow the instructions in the message to remedy the problem.

W0210006

[Message]

Saved RAM and register values to the file(xxx), but some RAM or register values are not saved due to some kind of problem.

[Explanation]

This message appears when saving of RAM or register values has failed.

[Action by User]

(1)

Check the emulator power.

(2)

Check whether the USB cable isn't cut.

(3)

Follow the instructions in the message to remedy the problem.

W0212001

[Message]

Overlaps xxx.

[Explanation]

et a size in the internal ROM size property that is different from other mapping areas. A value was set in the Mapping dialog box that overlaps with other mapping areas. xxx is a list of overlapping areas, separated by commas (,).

[Action by User]

Set the value so that it does not overlap with other areas.

W0212002

[Message]

The specified I/O protection area does not fit within single target memory area.

[Explanation]

The specified I/O protected area must fit inside a single configured target memory area. This message appears when the specified area protrudes from a single target memory area.

[Action by User]

Specify an area range that will fit inside a single target memory area.

W0220001

[Message]

Default docking layout has been restored because the invalid docking layout data specified.

[Explanation]

This message appears when restoring of the docking layout has failed.

[Action by User]

After adjusting the docking layout, save the layout again.

W0222001

[Message]

The list of microcontrollers has not been updated.

[Explanation]

This appears when an exception was thrown from the update library (such as when there are no updates or a restart is required).

[Action by User]

Follow the instructions in the message.

W0223001

[Message]

Source files were added to the Project Tree panel, but some files does not exist.

[Explanation]

When a debug project is downloaded, source files included in the load module are added automatically. This appears when any of the source files to be added are not on the file system.

[Action by User]

Add the source files manually to the Project Tree panel.

W0231001

[Message]

Specify the file to be downloaded.

[Explanation]

This message appears when, from the Download Files dialog box, the user clicks [OK] with the added download item file path left empty.

[Action by User]

Set the file path.

W0233001

[Message]

Could not move to the definition location of the function. Specify the function.

[Explanation]

Failed to move to the function definition specified in the Editor panel.

[Action by User]

Specify the function in the Editor panel.

W0235001

[Message]

The specified xxx does not exist.

[Explanation]

This appears when the user called the Go To The Location dialog box from the SFR/IOR panel, and a non-existent SFR/IOR name was specified.

[Action by User]

Specify an existing SFR/IOR.

W0238001

[Message]

The information of project files, the information of source files and the window images are output.

Remove these information if there is a confidential problem.

[Explanation]

This message appears in response to clicking on the [Record Screen] button in the Message dialog box.

W0240001

[Message]

Could not move to the definition location of the symbol. Specify the symbol.

[Explanation]

Failed to move to the definition of the specified symbol from the Disassemble panel.

[Action by User]

Specify the symbol in the Disassemble panel.

W0241001

[Message]

The trace number cannot be omitted.

[Explanation]

This message appears when saving trace data in the Data Save dialog box, and the [Save] button is clicked while the trace-number field is left blank.

[Action by User]

Enter a trace number in the field.

W0241002

[Message]

Enter a decimal value for the trace number.

[Explanation]

This message appears when saving trace data in the Data Save dialog box, and the [Save] button is clicked while a value other than a decimal number is in the trace-number field.

[Action by User]

Specify a decimal number in the trace-number field.

W0241003

[Message]

A trace number equal to or greater than the maximum trace number xxx has been specified.

[Explanation]

This message appears when saving trace data in the Data Save dialog box, and the [Save] button is clicked while a value greater than the maximum trace number is in the trace-number field.

[Action by User]

Specify a number no larger than the maximum trace number in the trace-number field.

W0242001

[Message]

The upper limit (128) of watch expressions that can be registered to the Watch panel has been exceeded.

[Explanation]

The maximum number of watch expressions that can be registered in a single Watch panel is 128.

[Action by User]

Remove unnecessary watch expressions or register it in a new Watch panel.

W0242002

[Message]

The upper limit (64) of categories that can be registered to the Watch panel has been exceeded.

[Explanation]

The maximum number of categories that can be registered in a single Watch panel is 64.

[Action by User]

Remove unnecessary categories or register it in a new Watch panel.

W0243001

[Message]

Cannot paste because the display format (notation system, bit width) is different.

[Explanation]

This message appears when pasting a memory value or ASCII characters in the Memory panel, and the display formats of the string to paste and the Memory panel are different (number base and bit width), and the paste can therefore not be performed.

[Action by User]

In the Memory panel, set the display format (number base and bit width) the same as the text to paste.

W0243002

[Message]

Characters that cannot be pasted in the [Memory Value Display] area are included.

[Explanation]

Illegal characters have been typed or pasted into the Memory panel's [Memory Value Display] area.

[Action by User]

Specify a string that can be treated as a memory value.

W0243003

[Message]

Only ASCII code can be pasted in the [Character Display] area.

[Explanation]

On the Memory panel, in the [Character Display] area, text can only be pasted when the encoding is specified as ASCII.

[Action by User]

Use the [Memory Value Display] area to paste text in other than ASCII encoding.

W0243004

[Message]

Cannot paste because the area contain write-protected area.

[Explanation]

This message appears when a memory value or ASCII characters are pasted into the Memory panel, and the area being pasted into is read-only.

[Action by User]

Change the length of text copied or the location copied to, in order to avoid pasting into a read-only area.

W0244001

[Message]

Too many initialization data.Only up to 16 initialization data can be specified.

[Explanation]

This message appears when 17 or more initial values are entered in the Memory Initialize dialog box, then the [OK] button is clicked.

[Action by User]

Set 16 or fewer initial values.

W0244002

[Message]

Each initialization data cannot exceed 4 bytes.

[Explanation]

This message appears when an initial value is 5 bytes or larger in size.

[Action by User]

Specify an initial value of no more than 4 bytes in size.

W0244003

[Message]

Enter the initialization data.

[Explanation]

This message appears when the initial data text box in the Memory Initialize dialog box is left empty, and the [OK] button is clicked.

[Action by User]

Enter initial values in the input box.

W0244004

[Message]

Enter the initialization data in hexadecimal.

[Explanation]

This message appears when non-hexadecimal values are entered in the initial data text box in the Memory Initialize dialog box.

[Action by User]

Enter initial values in the input box in hexadecimal format.

W0245001

[Message]

The search data cannot be omitted.

[Explanation]

When a search data input box of the Memory Search dialog box was in the state of the blank, and a [OK] button was clicked, it's shown to an error service provider.

[Action by User]

Input a character string to a search data input box.

W0245002

[Message]

The search data format is invalid. Specify with yyy of xxx.

[Explanation]

This appears in an error services provider when the format specified in the Memory Search dialog box differs from the notation or size shown in the Memory panel.

[Action by User]

Specify the data format displayed in the Memory panel in the search data.

W0245003

[Message]

Up to xxx bytes of data can be searched at one time.

[Explanation]

This appears in an error services provider when the specified size of data in the Memory Search dialog box exceeds the number of specified bytes.

[Action by User]

Specify data of the size less than the number of specified bytes.

W0245004

[Message]

An invalid character string has been entered. Enter a character string that can be encoded with xxx.

[Explanation]

This appears when characters are specified for a text search the Memory Search dialog box that cannot be displayed in the current encoding format of the Memory panel.

[Action by User]

Specify characters that can be encoded.

W0247001

[Message]

There is no available action event to set the specified location.

[Explanation]

This appears when the Action Events dialog box is opened, and there are no action events that can be configured.

[Action by User]

Specify a different location.

W0249001

[Message]

Clear out the category to be deleted.

[Explanation]

This message appears when a non-empty category is selected in the SFR/IOR panel, and the [Delete (EditDelete)] command is selected.

[Action by User]

Make the category empty.

In the SFR/IOR panel, delete the categories below the category you wish to delete, after moving SFR/IOR below them.

W0261001

[Message]

The segment name is invalid. The characters (0-9 A-Z a-z _ . / \\) can be used only.

[Explanation]

This appears when a segment name is specified in the Link Directive File Generation dialog box using illegal characters.

[Action by User]

Specify the segment name using valid characters.

W0261002

[Message]

A segment with the same name already exists.

[Explanation]

This appears when an existing segment name is specified in the Link Directive File Generation dialog box.

[Action by User]

Change the name of the segment to one that does not exist.

W0261003

[Message]

The section name is invalid. The characters (0-9 A-Z a-z _ . / \\) can be used only.

[Explanation]

This appears when a section name is specified in the Link Directive File Generation dialog box using illegal characters.

[Action by User]

Specify the section name using valid characters.

W0261004

[Message]

A section with the same name already exists.

[Explanation]

This appears when an existing section name is specified in the Link Directive File Generation dialog box.

[Action by User]

Change the name of the section to one that does not exist.

W0261005

[Message]

The symbol name is invalid. The characters (0-9 A-Z a-z _ . / \\) can be used only.

[Explanation]

This appears when a symbol name is specified in the Link Directive File Generation dialog box using illegal characters.

[Action by User]

Specify the symbol name using valid characters.

W0261006

[Message]

A symbol with the same name already exists.

[Explanation]

This appears when an existing symbol name is specified in the Link Directive File Generation dialog box.

[Action by User]

Change the name of the symbol to one that does not exist.

W0261007

[Message]

The section name is invalid. Specified name is a reserved section name for particular segment use only.

[Explanation]

This appears when a reserved section with a fixed segment is specified within a different segment in the Link Directive File Generation dialog box.

[Action by User]

Change the section to one that is not reserved.

W0261008

[Message]

The TP-symbol name is invalid. Specified TP-symbol name is no-exist.

[Explanation]

This appears in the case of a base TP symbol, when the TP specified in the Link Directive File Generation dialog box does not exist.

[Action by User]

Change to an existing TP symbol name.

W0261009

[Message]

The memory area name is invalid. The characters (0-9 A-Z a-z _ ? @) can be used only.

[Explanation]

This message appears when invalid characters have been used for the name of a memory area in the Link Directive File Generation dialog box.

[Action by User]

Only use valid characters for the names of memory areas.

W0261010

[Message]

A memory area with the same name already exists.

[Explanation]

This message appears when the name of an existing memory area has been specified in the Link Directive File Generation dialog box.

[Action by User]

Change the name of the memory area.

W0261012

[Message]

memory area range is invalid. Place the area without overlap to other memory area.

[Explanation]

This message appears when the address or size of a memory area specified in the Link Directive File Generation dialog box overlaps with that of an existing address range.

[Action by User]

Change the address or size of the memory area.

W0261013

[Message]

The start address of segment is invalid. Specify the address of the memory area to be placed.

[Explanation]

This message appears when the address of a segment specified in the Link Directive File Generation dialog box is outside the memory area to which the segment is to be allocated.

[Action by User]

Specify an address within the memory area to which the segment is to be allocated.

W0290001

[Message]

The Section field is empty.

Input a correct section name.

[Explanation]

This message appears when the section is empty.

[Action by User]

Enter a valid section.

W0290002

[Message]

Use only the following characters in the field except that 0-9 cannot be the first letter of a section name.

A-Z a-z 0-9 _ $ * ?

[Explanation]

This message appears when a string that is invalid as a section name is entered in an area for specifying a section name.

[Action by User]

Enter a valid section.

W0290003

[Message]

Use only the following characters in the field except that 0-9 cannot be the first letter of a symbol.

A-Z a-z 0-9 _ $

[Explanation]

This message appears when a string that is invalid as a symbol name is entered in an area for specifying a symbol name.

[Action by User]

Enter a valid symbol name.

W0290004

[Message]

The Address which is already specified cannot be specified again.

[Explanation]

This message appears when an address that has already been specified is specified again.

[Action by User]

Enter a unique address.

W0290005

[Message]

The Address field is empty.

Input an Address in the field.

[Explanation]

This message appears when the address is empty.

[Action by User]

Enter a valid address.

W0290006

[Message]

Please enter an integer.

[Explanation]

This message appears when a string that is invalid as an integer is entered in an area for specifying an integer value.

[Action by User]

Enter a string that represents a valid integer.

W0290007

[Message]

Please enter an integer between 0 and 0xffffff.

[Explanation]

This message appears when an out-of-bounds value is entered into an area for specifying an address.

[Action by User]

Enter a value within the range.

W0290008

[Message]

The 'Optimizes accesses to external variables' has been specified. Check 'Outputs the external symbol-allocation information file' in the Output category on the Link option tab.

[Explanation]

This appears when choosing the option which linked.

W0290009

[Message]

The specification of 'Optimizes accesses to external variables' has been canceled in all files in the project. Uncheck 'Outputs the external symbol-allocation information file' in the Output category on the Link option tab.

[Explanation]

This appears when choosing the option which linked.

W0290010

[Message]

The [Uses floating-point operation instructions] property is changed to [Depends on the CPU type option].

[Explanation]

This appears when choosing the option which linked.

W0290011

[Message]

Use only the following characters in the field.

A-Z a-z 0-9 @ _ . ∼ *

[Explanation]

This message appears when invalid characters have been detected in the field where a section name is specified.

[Action by User]

Enter a valid section name.

W0290012

[Message]

Please enter an integer between 0 and xxx.

[Explanation]

This message appears when an out-of-bounds value is entered into an area for specifying an address.

[Action by User]

Enter a value within the range.

W0290013

[Message]

Use only the following characters in the field.

A-Z a-z 0-9 @ _ . *

[Explanation]

This message appears when invalid characters have been detected in the field where a section name is specified.

[Action by User]

Enter a valid section name.

W0290015

[Message]

[Detect invalid indirect function call] has been changed. In synchronization with it, [Generate function list used for detecting invalid indirect function call] in the [Output] category on the [Link Options] tab is changed.

[Explanation]

This appears when choosing the option which linked.

W0291001

[Message]

The format of section or address is invalid.

[Explanation]

This message appears when a string with invalid format was entered when inputting a character string in [Specify a section start address] property in [Section] category in [Link Options] tab.

[Action by User]

Enter a string in accordance with the specified format.

W0291002

[Message]

Section Setting dialog does not support parentheses in option "start".

[Explanation]

This message appears when parentheses "()" are entered in [Specify a section start address] property in [Section] category in [Link Options] tab and the [...] button is clicked (instead of opening the Section Settings dialog box).

W0291003

[Message]

Specify valid rule number.

[Explanation]

This message appears when invalid characters have been detected in the field where MISRA-C rule numbers are specified.

[Action by User]

Enter valid rule numbers.

W0291004

[Message]

Specify valid predefined macro.

[Explanation]

This message appears when a predefined macro that is not specifiable was selected in [Invalidates the predefined macro] in [Source] category in [Compile Options] tab.

[Action by User]

Enter a valid predefined macro.

W0291005

[Message]

The following files cannot be specified as an excluded file. Project conversion continues, but following files are not registered to the project.

xxx

[Explanation]

This message appears at conversion of a HEW project in which a file type (cfg file) that cannot be specified as an excluded file was specified as an excluded file.

[Action by User]

[OK]:

Continue the conversion processing.

W0291006

[Message]

The value or the default value of the [Maximum byte count for data record] property exceeded the maximum limit.

The value and default value are changed to xxx.

[Explanation]

This message appears when "Motorola S type file(-FOrm=Stype)" was selected for the [Hex file format] property or "Yes" was selected for the [Specify byte count for data record] property for "Motorola S type file(-FOrm=Stype)", and the upper limit set as the default value or new value in the [Maximum byte count for data record] property was exceeded.

W0293001

[Message]

Watch your adding object/library files.

 

In some build mode, -Xwhole_program is set.

There is a possibility that an invalid code is made for adding the obj / lib file.Refer to the manual for details.

[Explanation]

This message appears when the -Xwhole_program option is set in build properties, and an .obj or .lib file is registered.

[Action by User]

Before using the -Xwhole_program option in build properties, make sure that none of the variables or functions to be compiled are referenced by external modules.

W0293002

[Message]

The 'Optimizes accesses to external variables' has been specified. Check 'Outputs the external symbol-allocation information file' in the Output category on the Link option tab.

[Explanation]

This appears when the compiler option -Omap is set in the CC-RH build properties, but the linker -MAp option is not set to "ON."

After displaying this warning, the build plug-in automatically enables the linker's -MAp option.

W0293003

[Message]

The specification of [Optimizes accesses to external variables] has been canceled in all files in the project. Uncheck [Output external symbol allocation information file] in the [Optimization(Details)] category on the Link option tab.

[Explanation]

This message appears when the selected option is used in conjunction with another option.

W0293004

[Message]

The file name is invalid. The characters ( \\ / : * ? " < > | ) cannot be used.

[Explanation]

This message appears when the filename includes invalid characters.

[Action by User]

Specify a valid filename.

W0293006

[Message]

xxx is used as a Boot Loader project for stand-alone debugging.

[Explanation]

This message appears when an active application project for a multicore is set as the configuration project of multiple boot loader projects while the [Priority debugging] property of each boot loader project is [Yes].

W0293007

[Message]

[Detect invalid indirect function call] has been changed. In synchronization with it, [Generate function list used for detecting invalid indirect function call] in the [Output code] category on the [Link Options] tab is changed.

[Explanation]

This appears when choosing the option which linked.

W0294001

[Message]

Watch your adding object/library file(s).

 

In some build mode, -Owhole_program is set.

There is a possibility that an invalid code is made for adding the obj / lib file. Refer to the manual for details.

[Explanation]

A file with the filename extension .obj or .lib has been added in a case where the -Owhole_program option is set in the build properties of the CC-RL.

[Action by User]

Before using the -Owhole_program option of the build properties of the CC-RL, ensure that there are no references from within external modules to functions and variables in the source files to be compiled.

W0294002

[Message]

The [Optimizes accesses to external variables] has been specified. Check [Output external symbol allocation information file] in the [Optimization(Details)] category on the Link option tab.

[Explanation]

The [Optimize access to external variables] option needs to be used in combination with the [Output external symbol allocation information file] option.

W0294003

[Message]

The specification of [Optimizes accesses to external variables] has been canceled in all files in the project. Uncheck [Output external symbol allocation information file] in the [Optimization(Details)] category on the Link option tab.

[Explanation]

Cancelling the [Optimize access to external variables] option also requires cancelling of the [Output external symbol allocation information file] option.

W0294004

[Message]

The file name is invalid. The characters ( \\ / : * ? " < > | ) cannot be used.

[Explanation]

The filename contains invalid characters.

[Action by User]

Specify a valid filename.

W0294005

[Message]

The specified value is out of range.

[Explanation]

A value outside the supported range has been entered in a field for numerical values (e.g. for a property setting).

[Action by User]

Enter a value within the supported range.

W0294006

[Message]

Specify valid contents of function information.

[Explanation]

This message appears when invalid characters have been detected in the field where contents of function information should be specified.

W0294007

[Message]

[Detect invalid indirect function call] has been changed. In synchronization with it, [Generate function list used for detecting invalid indirect function call] in the [Output code] category on the [Link Options] tab is changed.

[Explanation]

This appears when choosing the option which linked.

W0295006

[Message]

Options that the CS+ debugger doesn't support are specified.

xxx

[Explanation]

This message appears when you have specified a build tool option that the debugger running under CS+ does not support. xxx indicates the name of the option.

[Action by User]

Check the build tool options.

W0300001

[Message]

The name is already used. Please use another name.

[Action by User]

Change to a different name.

W0300002

[Message]

Only the user defined column can be deleted.

[Action by User]

Deselect non user-defined columns.

W0300003

[Message]

The column of the same name exists. Please input another name.

[Action by User]

Change the name.

W0300004

[Message]

Please input the column name.

W0300005

[Message]

Please select a column to delete.

W0300006

[Message]

The external peripheral of the same name exists. Please input another name.

[Action by User]

Change the name of the external peripheral.

W0300007

[Message]

Please input the external peripheral name.

W0300008

[Message]

The input value does not correspond to the type of the column. Please input a correct value.

[Action by User]

Change the value.

W0403000

[Message]

Code generation failed.

W0403001

[Message]

The following pin conflicts have been detected.

You must change the setting in that module before you can use it for other purpose.

W0403002

[Message]

Frequency of clock xxx is lower than clock yyy, you should change the setting in Clock Generator.

[RL78] No suitable value could be selected in valid range, please reset the peripheral clock in Clock Generator.

W0403003

[Message]

Please select the trigger.

W0403004

[Message]

Information of valid input value range: 0x00000000000000000000~0xfffffffffffffffffffx.

Input 10 byte Hex value.

W0403005

[Message]

Information of valid input value range: 16~238

The input value must be even.

W0403006

[Message]

Can not use uart for it needs two channels.

W0403007

[Message]

xxx is not selected now, and you should select the clock in Clock Generator before you want to use it.

W0403008

[Message]

Information of valid input value range: xxx~yyy

W0403009

[Message]

Source address range: xxx

W0403010

[Message]

Destination address range: xxx

W0403011

[Message]

The start-up file for the build object was changed to "xxx".

W0403012

[Message]

The link directive file for the build object was changed to "xxx".

W0403013

[Message]

The address will overflow as a result of counting direction and byte

W0403014

[Message]

The combination operation can't be selected, because its slave channel has been used for other purposes.

W0403015

[Message]

P52/SLTI/SLTO has been used by channel n.

W0403016

[Message]

Please firstly input valid xxx value.

W0403017

[Message]

Please input or select a valid SFR address.

W0403018

[Message]

When 20 MHz has been selected, the circuit cannot be changed to a 1 MHz internal high-speed oscillator.

W0403019

[Message]

The following interrupt conflicts have been detected.

You must change the setting in that module before you can use it for other purpose.

W0403020

[Message]

No channel can be used, please modify analog input pins selection.

W0403021

[Message]

xxx was changed, the following macros should be updated:yyy.

W0403022

[Message]

Cannot reflect user option byte to Code generator(Design Tool). Please change the value of user option byte or set it at Code Generator(Design Tool).

W0403023

[Message]

Cannot reflect build option to Code generator(Design Tool). Please change the setting of build option or Code Generator(Design Tool).

W0403028

[Message]

The xxx function shared by the yyy pin can be only used in input mode, using the port function in output mode is prohibited.

W0403029

[Message]

Please select pin assignment setting.

W0403030

[Message]

To use xxx module, please release yyy module firstly.

W0403031

[Message]

Please select the "xxx".

W0403032

[Message]

The following activation source conflicts have been detected.

W0403033

[Message]

To use xxx, please release yyy in zzz module firstly.

W0403034

[Message]

The following xxx conflicts have been detected.

W0403035

[Message]

Please set at least 2 slaves.

W0403036

[Message]

To use this selection, please unselect noise filter sampling clock from another channel.

W0403037

[Message]

Please set only 1 slave.

W0403038

[Message]

The combination operation can't be selected, because its master channel has been used for other purposes.

W0403039

[Message]

Please set master channel first.

W0403040

[Message]

Setting is not valid, because [xxx] is selected.

W0403041

[Message]

Setting is not valid, because no channel is used as analog input.

W0403042

[Message]

Setting is not valid, because [xxx] is changed.

W0403043

[Message]

Setting is not valid, because [High speed main mode] is not used in Clock Generator.

W0403044

[Message]

Please select one valid item.

W0403045

[Message]

Please input valid RAM address symbol.

W0403046

[Message]

There is an error in a set item. The source generation cannot be executed.

W0403047

[Message]

Input source setting is not valid.

W0403048

[Message]

To use xxx, please release yyy module firstly.

W0403049

[Message]

Comparator reference voltage is internal reference voltage, the temperature sensor output cannot be A/D converted.

W0403050

[Message]

Please select xxx (= yyy MHz) as zzz in Clock Generator before you want to use it.

W0403051

[Message]

Please input a valid text.

W0403052

[Message]

Oscillation stop detection can be used under either of the following conditions:

-

When bit 0 (WDSTBYON) and bit 4 (WDTON) of the option byte (000C0H) are set to 1 and bit 4 (WUTMMCK0) of the OSMC register is set to 0

-

When bit 4 (WUTMMCK0) of the OSMC register is set to 1

W0403053

[Message]

Please select xxx (yyy MHz) in Clock Generator before you want to use it.

W0403054

[Message]

Setting is not valid, because it has been set as analog input by ADPC register.

W0403055

[Message]

Setting is not valid, because it has been set as digital I/O by ADPC register.

W0403059

[Message]

Setting is not valid, because [Low voltage main mode] is used in Clock Generator.

W0403060

[Message]

Setting is not valid, because Comparators use as the cutoff function.

W0403061

[Message]

Frequency of clock xxx is less than clock yyy or zzz, please reset the peripheral clock in Clock Generator.

W0403062

[Message]

Frequency of clock xxx is less than clock yyy, please reset the peripheral clock in Clock Generator.

W0403063

[Message]

Setting is not valid, because Window A and Window B select the same channel.

W0403064

[Message]

Setting is not valid, because Upper-side level is less than Lower-side level.

W0403068

[Message]

Configuration file is loaded successfully.

W0403069

[Message]

This setting codes will be generated out in CG_CGC_Create because there is no related setting in xxx.

W0403070

[Message]

Could not set a valid value for #define xxx

W0403071

[Message]

The r_bsp_config.h has been changed externally, please click "Load" to update it into CGC

W0403072

[Message]

Couldn't find /r_config/r_bsp_config.h under current project

W0403073

[Message]

Couldn't find /r_bsp folder under current project

W0403074

[Message]

Please select the "xxx" or "yyy".

W0403075

[Message]

Setting is not valid, please change the selection in "xxx".

W0403076

[Message]

Frequency of clock xxx is lower than clock yyy, you should change the setting in System.

W0403077

[Message]

xxx is used as TAU input source.

W0403078

[Message]

Setting is not valid, because [System clock setting] in Clock Generator is changed.

W0403079

[Message]

To use this selection, please unselect "DA-AD synchronous" in DA module.

W0403080

[Message]

Please select one chip at least in the master.

W0403081

[Message]

Please select one scan group at least.

W0403082

[Message]

Because of pin conflict, pin group xxx can not be used.

W0403083

[Message]

Please select one DSADC channel at least.

W0403084

[Message]

Please select Replace input to xxx and yyy.

W0403085

[Message]

Please set 1 slave at least.

W0403086

[Message]

Please set the control data (DTCDn) for xxx chain transfers. (n is other than 23)

W0403087

[Message]

To use xxx, please use yyy firstly.

W0602102

[Message]

Please check connection of the exchange adapter.

W0603001

[Message]

Fewer than xxx or more than yyy characters cannot be specified.

[Explanation]

This message appears in the Message dialog box if a string is specified for the area that is shorter than xxx characters, or longer than yyy characters, when xxx and yyy are the minimum and maximum lengths, respectively.

[Action by User]

xxx is the minimum length of the character string, and yyy is the maximum length. The values of xxx and yyy are dependent on the input area.

W0603002

[Message]

More than xxx characters cannot be specified.

[Explanation]

This message appears when a line in the display source set in the Edit Text dialog box is longer than the maximum number of characters.

[Action by User]

Shorten the line that is greater than the maximum length so that it is within the maximum number of characters.

W0603003

[Message]

More than xxx lines cannot be specified.

[Explanation]

This message appears when the display source set in the Text Edit dialog box is longer than the maximum number of lines.

[Action by User]

Make sure that the number of lines is no more than the maximum limit.

W0603004

[Message]

Specify xxx digits in hexadecimal.

[Explanation]

This message appears when a string containing characters that cannot be used to represent a base-16 number is entered in a base-16 number field, or when the number of digits is not valid.

[Action by User]

Specify a hexadecimal number with <valid number of digits>.

W0603005

[Message]

This address expression is invalid. Check if the expression is correct or if the spelling of the symbols used in the expression is correct.

[Explanation]

This message appears when the start address or end address in the Memory Initialize dialog box is an invalid address expression.

W0603006

[Message]

Specify a numerical value.

[Explanation]

This message appears when a string containing characters that are invalid as numbers was entered in a numeric field.

[Action by User]

Specify a string that represents a valid number.

W0603007

[Message]

Specify in decimal.

[Explanation]

This message appears when a string containing characters that are invalid as a decimal number was entered in a decimal (base-10) numeric field.

[Action by User]

Specify a string that represents a valid number in decimal notation.

W0603008

[Message]

Fewer than xxx or more than yyy values cannot be specified.

[Explanation]

This message appears when an out-of-bounds value is entered into a numeric input area in the properties or the like.

[Action by User]

Specify a value between xxx and yyy.

W0603009

[Message]

Only ASCII character sets can be entered.

[Explanation]

This message appears when a string containing other than ASCII or numeric characters was entered in a field where only numbers or ASCII strings can be specified.

[Action by User]

Specify a string that is a valid number or a valid ASCII string.

W0603010

[Message]

Specify a character string.

[Explanation]

The field is empty.

[Action by User]

Specify a valid string.

W0603011

[Message]

Specify a path.

[Explanation]

The field is empty.

[Action by User]

Specify a valid path.

W0603012

[Message]

The specified path contains a non-existent folder.

[Action by User]

Specify a valid path.

W0603013

[Message]

The file name or path name is invalid. The characters ( \\ / : * ? " < > | ) cannot be used.

[Explanation]

The string includes illegal characters.

[Action by User]

Specify a valid filename or path.

W0603014

[Message]

The format is invalid.

[Explanation]

This message appears when a string with invalid format is entered into the properties or the like having a specific string format.

[Action by User]

Enter a string in accordance with the specified format.

W0603015

[Message]

Specify in hexadecimal.

[Explanation]

This message appears when a string containing characters that are invalid as a hexadecimal number was entered in a hexadecimal (base-16) numeric field.

[Action by User]

Specify a string that represents a valid number in hexadecimal notation.

W0603016

[Message]

Specify in decimal or hexadecimal.

[Explanation]

This message appears when a string containing characters that are invalid as a decimal/hexadecimal number was entered in a decimal (base-10)/hexadecimal (base-16) numeric field.

[Action by User]

Specify a string that represents a valid number in decimal/hexadecimal notation.

W0603017

[Message]

Enter a value smaller than the end address for the start address.

[Explanation]

This message appears when an area in which an address or symbol range is specified has a start address that is larger than the end address.

[Action by User]

Specify a start address that is less than or equal to than the end address.

W0603018

[Message]

Enter a value in the range of xxx to yyy.

[Explanation]

This message appears when a value greater than the address space of the debugging tool is specified in an area for an address or symbol range.

[Action by User]

Specify an address range that fits in the address space of the debugging tool.

W0603019

[Message]

The specified symbol does not exist.

[Explanation]

This message appears when a nonexistent symbol is specified in an area for an address or symbol range.

[Action by User]

Specify an existing symbol.

W0603020

[Message]

The address cannot be omitted.

[Explanation]

This message appears when an area for an address/symbol is left blank, and blank entries are not allowed.

[Action by User]

Specify an address, symbol, or address expression.

W0603021

[Message]

The character string is too long. Specify a character string with xxx or fewer characters.

[Explanation]

This message appears when a string was specified in a string area that was longer than the maximum length.

[Action by User]

Specify a string of no more than the maximum number of characters.

W0603022

[Message]

The address expression is invalid. Specify a symbol or numerical value.

[Explanation]

This message appears when a string that is invalid as an address expression is entered in an address-expression area.

[Action by User]

Specify a string that is correct as an address expression.

W0603030

[Message]

The load module which linked the flash library not found.

W0603032

[Message]

Specify the address of the 1MB boundary unit as the starting address of coverage measurement area.

W0603034

[Message]

Specified value is already set.

W0603035

[Message]

Changed the trace target, because debug mode has been changed. If you want to change the trace target, change the "trace target" property.

W0603036

[Message]

Changed to enable the security function. If enable the security function, can not be returned disabled.

W0615000

[Message]

The upper limit (xxx) of categories that can be registered to the Watch panel has been exceeded.

[Action by User]

Ensure that the number of categories registered in one Watch panel is no greater than the upper limit.

W0615001

[Message]

The upper limit (xxx) of watch expressions that can be registered to the Watch panel has been exceeded.

[Action by User]

Ensure that the number of watch-expressions registered in one Watch panel is no greater than the upper limit.

W0617000

[Message]

Set OPJTAG in LPD for debug tool connection.

[Action by User]

The debug tool forcibly changes the OPJTAG setting to select LPD upon its connection to CS+.

If you set the [Set OPJTAG in JTAG connection before disconnecting] property to [Yes], the JTAG connection will be restored after the debug tool is disconnected.

W0810001

[Message]

A variable or a register with the input name doesn't exist.

W0805001

[Message]

Specify in decimal.

[Explanation]

This message appears when a string containing characters that are invalid as a decimal number was entered in a decimal (base-10) numeric field.

[Action by User]

Specify a string that represents a valid number in decimal notation.

W0805002

[Message]

Specify in decimal or hexadecimal.

[Explanation]

This appears when an area specifying a decimal/hexadecimal number includes characters that cannot be used to represent a decimal/hexadecimal number.

[Action by User]

Specify a string that represents a valid number in decimal/hexadecimal notation.

W0805003

[Message]

The character string is too long. Specify a character string with xxx or fewer characters.

[Explanation]

This message appears when a string was specified in a string area that was longer than the maximum length.

[Action by User]

Specify a string of no more than the maximum number of characters.

W0805004

[Message]

Please input a value that is smaller than the upper bound value to lower bound value.

[Explanation]

This message appears when entering the lower limit of the display range of an analysis graph or the lower limit of its valid range, and the sizes of the upper and lower limits are reversed.

[Action by User]

Enter a lower limit that is smaller than the upper limit.

If you will also enter a larger upper limit, enter the value for the upper limit first.

W0805005

[Message]

Please input a value that is bigger than lower bound value to the upper bound value.

[Explanation]

This message appears when entering the upper limit of the display range of an analysis graph or the upper limit of its valid range, and the sizes of the upper and lower limits are reversed.

[Action by User]

Enter a upper limit that is larger than the lower limit.

If you will also enter a smaller lower limit, enter the value for the lower limit first.

W0805008

[Message]

Fewer than xxx or more than yyy values cannot be specified.

[Explanation]

This message appears when an out-of-bounds value is entered into a numeric input area in the properties or the like.

[Action by User]

Specify a value between xxx and yyy.

W0805009

[Message]

The file name or path name is invalid. The characters ( \\ / : * ? " < > | ) cannot be used.

[Explanation]

The string includes illegal characters.

[Action by User]

Specify a valid path name.

W0820001

[Message]

Unknown destination.

[Explanation]

This message appears when a destination is unknown when executing the [Jump to Source] menu command, etc..

It is not possible to jump from specified location, because a destination is unknown.

W0827001

[Message]

Can not preview image.

[Explanation]

This message appears when the generation of preview images was not possible due to the project having too many functions or another reason.

W1200723

[Message]

The specified trace-buffer size has been reduced due to memory shortage.

W1203106

[Message]

Memory unready status was canceled.

W1204111

[Message]

Target is not turned on.

W1204116

[Message]

Data is not exist.

W1208205

[Message]

No initialize data for SFR/IOR.

W1216412

[Message]

Software break can not be set on this area.

W1220491

[Message]

Specified device file does not relocate internal RAM.

W1220494

[Message]

No tag data which it was going to refer to device file.

W1228688

[Message]

No source information exists.

W1228689

[Message]

Unknown result of step execution.

W1245086

[Message]

No debug information (not compiled by the method of generating debug information).

W1245110

[Message]

Out of variable region.

W1245122

[Message]

Symbol module is not initialized.

W1245877

[Message]

Too long symbol name.

W1249175

[Message]

Symbol information is duplicated, please reset symbols.

W1249178

[Message]

BSS area is assigned to non-mapped area.

W1249180

[Message]

Programmable IOR address mismatch.

W1249181

[Message]

Selected load module different from kind(Chip) was loaded.

W1790000

[Message]

The timer overflow.

W1790001

[Message]

The timer function is not supported.

W1810204

[Message]

USB bus power voltage is low.

[Action by User]

Change the host machine.

W1811110

[Message]

Warning: MDE bit of MDE register was modified.

W1811111

[Message]

UB code was modified.

W1811112

[Message]

MDE register and UB code are modified.

W1811115

[Message]

Started up with hot plug-in, but option setting memory is not written.

[Action by User]

To set up the option-setting memory, start up the emulator and download a file with the required settings.

W1811126

[Message]

Warning: OSF1 register value was modified.

[Explanation]

This message only appears during debugging. Data was modified.

W1811127

[Message]

Warning: MDE bit of MDE register value and OFS1 register value were modified.

[Explanation]

This message only appears during debugging. Data was modified.

W1811128

[Message]

Warning: BANKMD bit of MDE register value were modified.

W1811129

[Message]

Warning: BANKSWP bit of BANKSEL register value were modified.

W1811130

[Message]

Warning: MDE bit and BANKMD bit of MDE register value were modified.

W1811131

[Message]

Warning: MDE bit and BANKMD bit of MDE register value, BANKSWP bit of BANKSEL register value were modified.

W1811132

[Message]

Warning: BANKMD bit of MDE register value, BANKSWP bit of BANKSEL register value were modified.

W1811133

[Message]

Warning: BANKMD bit of MDE register value, OFS1 register value were modified.

W1811134

[Message]

Warning: MDE bit and BANKMD bit of MDE register value, BANKSWP bit of BANKSEL register value were modified.

W1811135

[Message]

Warning: MDE bit and BANKMD bit of MDE register value, OFS1 register value were modified.

W1811306

[Message]

The read operation to the data flash area where reading was prohibited occurred.

W1811318

[Message]

The access violation to the internal flash ROM has occurred (ILGLERR bit is '1').

W1811321

[Message]

Data for MDE register was modified for the endian, which was specified on starting up.

W1811322

[Message]

Data for UB code was modified for the operating mode, which was specified on starting up.

W1811323

[Message]

Data for MDE register and UB code were modified for the setting, which was specified on starting up.

W1811325

[Message]

Internal ROM area was accessed while user program is running.

W1811326

[Message]

The emulator has recovered from a communication error which occurred because the clock was switched during memory access or due to other reasons.

W1811328

[Message]

Warning: The writing data for OFS1 register was modified to disable "Voltage Monitoring Reset".

[Explanation]

This message only appears during debugging. Data was modified.

W1811329

[Message]

It is unable to enable the "Voltage Monitoring Reset".

W1811330

[Message]

Warning: The area where CPU access is needed was accessed while the program is running.

[Explanation]

This message only appears during debugging. The debugger is not allowed to read data from the CPU-access area while the user program is running.

W1811333

[Message]

Warning: The writing data for OFS1 register was modified to disable "Voltage Monitoring Reset".

[Explanation]

Ensure that the voltage monitoring reset is disabled after a reset.

W1811334

[Message]

Warning: There's no data for option setting memory.

[Action by User]

Specify the values to be set for the option-setting memory in the file for downloading.

W1811336

[Message]

Warning: The download data were not written in the Trusted Memory area.

[Explanation]

The area for the downloading of data includes locations in the Trusted Memory area.

[Action by User]

Ensure that the area for the downloading of data does not include any locations in the Trusted Memory area.

W1811337

[Message]

Warning: The wait setting for the RAM was changed temporarily to access it correctly.

[Explanation]

The memory-wait cycle setting is incorrect.

[Action by User]

Check the memory-wait cycle setting.

W1811338

[Message]

Warning: The wait setting for the ROM was changed temporarily to access it correctly.

[Explanation]

The memory-wait cycle setting is incorrect.

[Action by User]

Check the memory-wait cycle setting.

W1811341

[Message]

The writing data for FSPR bit in the FAW register was modified to without protection.

W1811342

[Message]

Protection by FSPR bit in the FAW register has already been set.

W1811343

[Message]

Warning: Data for BANKMD bit of MDE register were modified for the setting, which was specified on starting up debugger.

W1811344

[Message]

Warning: Data for BANKSWP bit of BANKSEL register were modified for the setting.

W1811345

[Message]

Warning: Data for MDE register or BANKMD register were modified for the setting, which was specified on starting up debugger.

W1811346

[Message]

Warning: Data for MDE bit and BANKMD bit of MDE register were modified for the setting, which was specified on starting up debugger.

W1811347

[Message]

Warning: Cannot modify BANKSWP bit of BANKSEL register, because the TM function is enable and the TM function of FFEE0000h to FFEEFFFFh is disable.

W1812808

[Message]

There was a sector that could not be written/erased in the external flash ROM, because it was locked.

W1812910

[Message]

Warning: While E2 expansion function is running, power from emulator cannot be supplied.

W1891371

[Message]

Order of the sequential event might have been modified. Please check the detail setting of the event combination.

[Action by User]

Set the event sequence again by editing the combination of conditions.

W1891901

[Message]

Because the value of the operating frequency has not been set, 25.0MHz is used as its initial value. The timer measurement result may be incorrect.

W1892250

[Message]

Register ID is invalid.

[Action by User]

Specify the correct register ID.

W1892251

[Message]

The specified value is over the maximum value which can be set to the register.

[Action by User]

Enter a value within the specifiable range.

W2000001

[Message]

The function xxx cannot be found.

[Explanation]

This message dialog box appears when the selected function name cannot be jumped to using the "Jump to function" operation.

[Action by User]

Check whether the function of the name at the cursor position exists in the project.

Check whether the program was built with the cross reference information output. (Usually if the function name is displayed in the function list, the cross reference information has been output.)

W2000003

[Message]

The symbol or address xxx cannot be found.

[Explanation]

This message appears when the given symbol or address was not found, so jumping to the location of the symbol or the address was not possible.

[Action by User]

Check whether the symbol exists in the project.

Check whether the address is within the address range (code section range) displayable by the editor.

Check whether the program was built with the cross reference information output. (Usually if the symbol is displayed in the function list or variable list, the cross reference information has been output.)

W2200001

[Message]

option-name is unknown option, ignore.

[Explanation]

The specified option is not supported.

The setting is ignored and processing is continued.

W2200006

[Message]

Block information file not found.

[Explanation]

This message appears when the file specified by the -iorblock option cannot be found.

[Action by User]

Check if the information file that defines blocks exists.

W2200007

[Message]

Cannot read block information file (unknown file).

[Explanation]

Loading of the information file that defines blocks has failed. A file that is not the information file that defines blocks was specified.

[Action by User]

Specify the information file that defines blocks.

W2200008

[Message]

An IOR block has unknown format, ignore.

[Explanation]

This message appears when the format of definition information of one block is illegal in the information file that defines blocks.

[Action by User]

Confirm that the information file that defines blocks is a legitimate file.

W2300001

[Message]

Stop checking in the middle because the size of the buffer for the exclusive control checking tool has been exceeded.

[Explanation]

This message appears when more than 10,000 software trace instructions are stored into the buffer for the exclusive control check tool.

[Action by User]

Limit the range to be checked for the exclusive control check tool.

W2441337

[Message]

(Warning message)

The wait setting of RAM was changed temporarily to execute this command.

W2441338

[Message]

(Warning message)

The wait setting of ROM was changed temporarily to execute this command.