This tab displays information on each pin of the microcontroller in the order of pin number.
The following items are explained here.
On the Project Tree panel, double-click [Project name (Project)] >> [Code Generator (Design Tool)] >> [Pin View] >> [Device List View]. |
On the Project Tree panel, select [Project name (Project)] >> [Code Generator (Design Tool)] >> [Pin View] >> [Device List View], and then press the [Enter] key. |
This area displays the “device list view” for entering information on the pins of the microcontroller.
The device list view in this area is organized in the order of pin number.
The following are the columns comprising the device list view.
This area allows you to select “which function to use” when the pin has more than one functions. |
|
Displays the comment of the pin Comments can be arbitrarily set up by 200 characters or less |