PerformanceInfo


This class holds performance measurement information (return value of the debugger.Performance.Get function). [RH850][E1/E2/E20/Full-spec emulator]

[Type]

class PerformanceInfo:
        Number = 0
        Count = 0
        Mode = PerformanceMode.MaxCount
        Item = PerformanceItem.AllFetchCall
        IsOverflow = False

[Variable]

Variable

Description

Number

This holds the performance measurement event number.

Count

This holds the number of times it was counted.

PerformanceMode

This holds the mode for performance measurement.

Mode

Description

PerformanceMode.PassCount

Pass count

PerformanceMode.NewCount

New count

PerformanceMode.MinCount

Min count

PerformanceMode.MaxCount

Max count

PerformanceMode.AddCount

Total count

PerformanceItem

This holds performance measurement items.

Item

Description

PerformanceItem.FlashRomDataRequest

Flash ROM data request count

PerformanceItem.CpuFetchRequestHit

Response count for CPU issued instruction fetch request

PerformanceItem.CpuFetchRequest

CPU issued instruction fetch request count

PerformanceItem.DisableInterruptCycle

Interrupt disable cycle of DI/EI

PerformanceItem.NoInterruptCycle

Non-interrupt cycle

PerformanceItem.ClockCycle

Clock cycle

PerformanceItem.ALLInstructionSyncException

All instruction sync exception count

PerformanceItem.AllInstructionAsyncException

All instruction async exception count

PerformanceItem.FetchFELevelInterrupt

FE level interrupt count

PerformanceItem.FetchEILevelInterrupt

EI level interrupt count

PerformanceItem.AllFetchBranch

Branch instruction count

PerformanceItem.AllFetchCall

All instruction count

[Detailed description]

-

PerformanceInfo is a class, and it is passed as the return value when the debugger.Performance.Get function is executed.