This class holds disassembly information (return value of the debugger.Assemble.Disassemble function).
[Type]
class DisassembleInfo:
Address = 0
Code = None
Mnemonic = None
|
[Variable]
|
|
|
|
Address
|
This holds the address.
|
|
Code
|
This holds code information as a collection of bytes.
|
|
Mnemonic
|
This holds mnemonic information.
|
[Detailed description]
[Example of use]
>>>info = debugger.Assemble.Disassemble("main", 4) ...Disassemble command
0x000002DC B51D br _main+0x36
0x000002DE 0132 mov0x1, r6
0x000002E0 60FF3800 jarl _func_static1, lp
0x000002E4 63570100 st.w r10, 0x0[sp]
>>>print info[0].Address
732
>>>print info[0].Code[0]
181
>>>print info[0].Code[1]
29
>>>print Mnemonic
br _main+0x36
>>>print info[3].Address
740
>>>print info[3].Code[0]
99
>>>print info[3].Code[1]
87
>>>print info[3].Code[2]
1
>>>print info[3].Code[3]
0
>>>print info[3].Mnemonic
st.w r10, 0x0[sp]
>>>
|