This function initializes Python.
[Specification format]
common.PythonInitialize(scriptFile = "")
|
[Argument(s)]
|
|
scriptFile
|
Specify the script file to run after initializing Python (default: not specified).
Specify the absolute path.
|
[Return value]
None
[Detailed description]
- | This function initializes Python.
Initialization is performed by discarding all defined functions or imported modules. If this function is executed while executing a script, Python is forcibly initialized regardless of the execution state.
|
- | If a script file is specified in scriptFile, the specified script file is executed after initialization has finished. |
- | If scriptFile is not specified, Python is merely initialized. |
Caution | Since Python is forcibly initialized, an error may be displayed depending on the execution state. |
[Example of use]
>>>common.PythonInitialize()
>>>
>>>common.PythonInitialize("C:/Test/script.py")
|