This function sets measurement conditions of a conditional timer. [RH850][E1/E20/Full-spec emulator]
[Specification format]
debugger.Timer.Detail(timerNumber = "", timerOption)
|
[Argument(s)]
|
|
|
|
timerNumber
|
Specify the timer event number for which you wish to set measurement conditions.
|
|
timerOption
|
Set measurement conditions of a conditional timer.
|
|
|
|
|
|
TimerOption.PassCount
|
RH850
|
Pass count
|
|
TimerOption.MinCount
|
RH850
|
Minimum count
|
|
TimerOption.MaxCount
|
RH850
|
Maximum count
|
|
TimerOption.AddCount
|
RH850
|
Add count
|
[Return value]
If setting measurement conditions of a conditional timer was disabled successfully: True
If there was an error when setting measurement conditions of a conditional timer: False
[Detailed description]
- | This function sets measurement conditions of the timer event number specified by timerNumber. |
- | If timerNumber is not specified, then measurement conditions of all timer events will be set. |
[Example of use]
>>>debugger.Timer.Information()
1 Timer Result1 Enable 0x00001000 - 0x00002000
2 Timer Result2 Enable 0x00003000 - 0x00004000
>>>debugger.Timer.Detail(1, TimerOption.PassCount) …Change the timer measurement condition to pass count
True
>>>
|
>>>debugger.Timer.Detail(TimerOption.MaxCount) …Change the timer measurement condition of all timer events to maximum execution time
True
>>>
|