This function displays the current IE status.
[Specification format]
[Argument(s)]
None
[Return value]
Current IE status (string)
|
|
Break
|
Break in effect
|
Coverage
|
Coverage running
|
Timer
|
Timer running
|
Tracer
|
Trace running
|
Step
|
Step executing
|
Run
|
User program running
|
RunOrStep
|
User program running or step executing
|
Caution | If a PM+ workspace is converted to a CS+ project, then there will be no debugging tool in the main project. For this reason, "None" will be returned if the main project is the active project.
In addition, "None" will be returned before the debugging tool is connected.
|
[Detailed description]
- | This function displays the current IE status. |
[Example of use]
>>>debugger.GetIeStatus()
Run
>>>
|