|
build.Link.SectionAlignment
|
This property sets or refers to the link options for the active project regarding section alignment. [CC-RH][CC-RX][CC-RL]
[Specification format]
build.Link.SectionAlignment = sectionlist
|
[Setting(s)]
|
|
|
|
sectionlist
|
Set section alignment as a list of strings.
|
[Reference]
List of section alignment
[Detailed description]
- | This property sets or refers to the link options for the active project regarding section alignment. |
- | Add or change for the referred list to change the setting. |
[Example of use]
>>>lib1 = build.Link.LibraryFile ... Refer the current setting and add section alignment
['R_1']
>>>sec1.append('R_2')
>>>build.Link.SectionAlignment = sec1
>>>print build.Link.SectionAlignment
['R_1', 'R_2']
>>>
>>>sec2 = ['R_1', 'R_2'] ... Set multiple section alignment
>>>build.Link.SectionAlignment = sec2
>>>print build.Link.SectionAlignment
['R_1', 'R_2']
|