Building and Downloading a Program

Let us rebuild the program after creating sample project, and download the load module to simulator.

Click [Rebuild Project] button, and then click [Download] button.

Layouts of main display get changed.

Now, the preparing for trying analysis features is finished.

Tip

To use an analysis function, it's necessary to output information for analyses in a build tool.

Build after setting "Enable static analysis information" as "Yes." and "Enable dynamic analysis information" as "Yes." in a property of analysis tool.

The sample project is made setting of "Yes.".