Procedure to Create a Program

This section describes a procedure to create a program.

Start performing the task after installing CS+.

(1) Open the sample program

:This time, you dont use the code-generation functions. Instead, you must read out a program from a sample program.

(2) Coding

:Since you use a sample program, you dont edit the program. Here, we describe how to perform basic operations.

(3) Build

:Build the program

(If an error occurs, edit the program again).

(4) Debugging

:Debug the program using R0K556100S000BE

and E1.

(5) Writing

: Write a program to the microcontroller using E1