Starting CS+

2. Open the sample Project

In this step, you configure the information necessary to create a project.

In the "Load Sample Project" field, from the "RX" tab, select "RX610_Tutorial_Basic_Operation", then click [GO].

Follow the on-screen instructions. A sample program opens as shown in the figure below.