[General - Display] category


Use this category to configure general settings relating to program messages.

Figure A.43

Option Dialog Box ([General - Display] Category)

 

The following items are explained here.

[How to open]

-

From the [Tool] menu, select [Options...].

[Description of each area]

(1)

[Message dialog box display level]

Select the Message dialog box display level (verbosity) from the following drop-down list.

Regardless of this setting, all messages are displayed in the Output panel.

Information, warning and error

Displays all messages in a Message dialog box.

Warning and error

Displays warning and error messages in a Message dialog box (default).

Error only

Only displays error messages in a Message dialog box.

Fatal error only

Only displays fatal error messages in a Message dialog box.

(2)

[Toolbar display type]

Use this area to select the format in which to display toolbars on each panel, via the following drop-down list.

Icon only

Displays icons only (default).

Icon and label

Displays both icons and labels (text).

(3)

[Show function key commands]

 

Displays the Function Key bar in the Main window (default).

 

Does not display the Function Key bar in the Main window.

(4)

[Show window contents while resizing]

 

Resizes the window while displaying areas that were not visible before.

 

Resizes the window without displaying areas that were not visible before (default).

(5)

[Tab width]

Specify the number of tab columns.

Either enter a number between 1 and 16 directly via the keyboard, or specify a number via the buttons. The default is 8.

Note that clicking on the [OK] or [Apply] button while this item remains blank causes the tab setting to remain at the previously saved value.

(6)

[Select the file opened with text editor in project tree]

 

When the Editor panel is activated, the file currently being opened is selected in the Project Tree panel (default).

 

Even if the Editor panel is activated, the file currently being opened is not selected in the Project Tree panel.

(7)

[Show overlay icons for Windows Explorer in project tree]

 

Displays overlay icons for Windows Explorer in the Project Tree panel.

 

Does not display overlay icons for Windows Explorer in the Project Tree panel (default).

Caution

The change of the setting is reflected after this product restarts.

(8)

[Location of a close button for a splitted panel]

Use this area to select the location of a close button for a split panel, via the following drop-down list.

Right edge of the tab area

Displays to the right edge in the tab area (default).

All tabs

Displays to the right edge of the title in all tabs.

Active tab

Displays to the right edge of the title in the active tab.

(9)

Buttons

Initialize Settings

Returns all currently displayed setting to their default values.

[Function buttons]

Button

Function

Initialize All Settings

Restores all settings on this dialog box to their default values.

Note, however, that newly added items in the [General - External Tools] category will not be removed.

OK

Applies all setting and closes this dialog box.

Cancel

Ignores the setting and closes this dialog box.

Apply

Applies all setting (does not close this dialog box).

Help

Displays the help of this dialog box.