[Commands] tab


You can customize items to include on a toolbar or a menu.

Figure A.63

User Setting Dialog Box: [Commands] Tab

 

The following items are explained here.

[How to open]

-

From the [Tool] menu, select [User Setting...].

[Description of each area]

(1)

[Categories] area

Display a list of the categories of commands that CS+ provides.

(2)

[Commands] area

Display a list of the names of commands belonging to the category selected in the [Categories] area, together with their icons (if exist).

When "(All Commands)" is selected in the [Categories] area, the name of all commands that CS+ provides are displayed, together with their icons (if exist).

To add a command on a toolbar/menu, drag and drop the command name in this area onto the toolbar/menu displayed in the actual Main window.

(3)

Buttons

Modify Selection

In order that the menu item or the button on a toolbar currently selected in the Main window, displays the following menu items beneath this button:

Menu Item

Description

Reset

Resets the selected menu item/button.

Delete

Deletes the selected menu item/button.

Name

Displays the name of the selected menu item/button.

Default Style

Checking this menu item returns the display style of the selected menu item/button to the default state (by default).

Text Only (Always)

Checking this menu item displays the selected menu item/button by text only (the icon will not be displayed).

Text Only (in Menu)

This is enabled only when a menu item is selected. Checking this menu item displays the selected menu item/button by text only (the icon will not be displayed).

Image and Text

Checking this menu item displays the selected menu item/button by both text and icon.

Begin a Group

Inserts separator just before the selected menu item/button.

Recently Used

This item is not supported in this version.

Rearrange Commands...

Opens the Rearrange Commands dialog box for changing the arrangement (including addition and deletion) of menu items and tool bar buttons in the Main window.

[Function buttons]

Button

Function

Keyboard...

Opens the Customize Keyboard dialog box to assign customized items to keys on the keyboard.

Close

Cancels the toolbar/menu customization setting and closes this dialog box.