D.2 Displaying Icons at Locations of Input Errors

In some of the panels and dialog boxes provided by CS+, the icon will appear at a point where incorrect characters are entered or a required item is missing.

Remark

Placing the cursor over the icon will pop up the information that indicates the characters to be entered (tips to fix the error).

Figure D.1

Sample Icons Shown at Locations of Input Errors