2.4.2 Filtering of analysis information
To filter analysis information, use the Filtering menu which is displayed by clicking on the
icon located in the column header in the
Analysis information table area.
Table 2-2. Filtering Menu
|
|
|
|
|
Displays all analysis information.
|
|
|
Opens the Filter Settings dialog box that sets a filter condition on analysis information which is displayed as a CPU usage status.
|
|
|
Only displays the lines indicated by "-".
|
|
|
Displays lines other than those indicated by "-".
|
|
|
Only displays the target object lines.
|
Figure 2-4. Filter Settings Dialog Box
(1) Filtering using one filter condition
Remarks 1. When performing filtering using one filter condition, set the combo box in the
2nd filter condition setting area (left side) to "blanks", and the combo box (right side) to "no condition".
(2) Filtering using two filter conditions