2.3
Set Trace Start Event
Set a trace start event that enables CS+ to acquire trace data when the execution of the load module is started.
A trace start event can be set by pressing the
button which is located on the Toolbar on the Realtime OS Task Analyzer panel.
|
|
|
|
|
Indicates that a trace start event is not set. When the button is in this condition, no trace data is acquired when the execution of the load module starts.
|
|
|
Indicates that a trace start event is set. When the button is in this condition, trace data is acquired when the execution of the load module starts.
|