2.14 Save Analysis Information

You can save the contents of the Function List panel, Variable List panel, Analysis Chart panel, Call Graph panel, and Variable Value Changing Chart (zoomed in) panel to a file.

(1)

Save function information

To do this, with the focus on the Function List panel, select [Save Function List Data As...] from the [File] menu. The Save As dialog box opens; perform the operation from this dialog.

The following file formats can be specified when saving the information.

Text file (*.txt)

Text format

CSV(Comma-Separated Variables) (*.csv)

CSV format

Microsoft Office Excel Workbook (*.xls)

Microsoft Office Excel book format

Function List file (*.mtfl)

File format to import the function information (see "2.12 Import or Export Information File".)

Caution

Only the items/analysis information currently displayed in the panel can be saved.

(2)

Save variable information

To do this, with the focus on the Variable List panel, select [Save Variable List Data As...] from the [File] menu. The Save As dialog box opens; perform the operation from this dialog.

The following file formats can be specified when saving the information.

Text file (*.txt)

Text format

CSV(Comma-Separated Variables) (*.csv)

CSV format

Microsoft Office Excel Workbook (*.xls)

Microsoft Office Excel book format

Variable List file (*.mtvl)

File format to import the variable information (see "2.12 Import or Export Information File".)

Caution

Only the items/analysis information currently displayed in the panel can be saved.

(3)

Save graph information

To do this, with the focus on the Analysis Chart panel, select [Save Analysis Chart Data As...] from the [File] menu, or with the focus on the Variable Value Changing Chart (zoomed in) panel, click the [Save] button. The Save As dialog box opens; perform the operation from this dialog.

The following file formats can be specified when saving the information.

Text file (*.txt)

Text format

CSV(Comma-Separated Variables) (*.csv)

CSV format

Microsoft Office Excel Workbook (*.xls)

Microsoft Office Excel book format

Analysis Chart Data (*.mtac)Note 1

Analysis chart data file

Bitmap (*.bmp)

Bitmap format (32-bit) (graphic file format)

JPEG (*.jpg)

JPEG format (graphic file format)

PNG (*.png)

PNG format (graphic file format)

EMF(*.emf)Note 2

EMF format (Graphic file format)

Notes 1.

This format is only applied to the [Variable Value Changing Chart] tab of the Analysis Chart panel.

Notes 2.

Only the area of graph rendering is saved (trigger marks, channel information, etc. cannot be saved).

Cautions 1.

For the Analysis Chart panel, only the contents of the currently displayed tab will be saved.

Cautions 2.

When the graphic file format is selected, only the part currently being displayed in the panel will be saved.

(4)

Save call graph information

To do this, with the focus on the Call Graph panel, select [Save Call Graph Data As...] from the [File] menu. The Save As dialog box opens; perform the operation from this dialog.

The following file formats can be specified when saving the information.

Note that when "(Only the visible part)" is selected, only the part currently being displayed in the panel will be saved.

Bitmap(Only the visible part) (*.bmp)

Bitmap format (32-bit) (graphic file format)

JPEG(Only the visible part) (*.jpg)

JPEG format (graphic file format)

PNG(Only the visible part) (*.png)

PNG format (graphic file format)

Bitmap (*.bmp)

Bitmap format (32-bit) (graphic file format)

JPEG (*.jpg)

JPEG format (graphic file format)

PNG (*.png)

PNG format (graphic file format)

EMF (*.emf)

EMF format (graphic file format)

Caution

All part of the call graph may not successfully be saved as a graphic file format if the project is too big.

Remark

If the zoom function has been applied, then the image will be saved at the current zoom ratio (except for EMF format).