The macros supported in the CA78K0 are converted as follows. If there is no corresponding macro in the CC-RL, the CcnvCA78K0 outputs a message. The CPU macro is not converted and no message is output.
 
| 
Table 3.1 | Conversion of Macro Names | 
|  |  |  | 
| 
__LINE__ | 
Not converted | 
Can be used in the CC-RL without any change. | 
| 
__FILE__ | 
Not converted | 
Can be used in the CC-RL without any change. | 
| 
__DATE__ | 
Not converted | 
Can be used in the CC-RL without any change. | 
| 
__TIME__ | 
Not converted | 
Can be used in the CC-RL without any change. | 
| 
__STDC__ | 
Not converted | 
Can be used in the CC-RL without any change. | 
| 
__K0__ | 
Not converted | 
A message is output. 
Handled as a user-defined macro in the CC-RL. | 
| 
__STATIC_MODEL__ | 
Not converted | 
A message is output. 
Handled as a user-defined macro in the CC-RL. | 
| 
__CHAR__UNSIGNED__ | 
__UCHAR | 
  | 
| 
__CA78K0__ | 
Not converted | 
A message is output. 
Handled as a user-defined macro in the CC-RL. | 
| 
CPU macro | 
Not converted | 
A message is not output. 
Handled as a user-defined macro in the CC-RL. |