When the message number type is information, the information types are classified as follows.
| 
Table 4.2 | Information Types | 
|  |  | 
| 
Change | 
Changes were made in the program so that it can be handled by the CC-RL. | 
| 
Insert | 
Additions were made in the program so that it can be handled by the CC-RL. | 
| 
Delete | 
Some descriptions were deleted because they are not necessary in the CC-RL. | 
| 
Info | 
Conversion may not be sufficient in some cases because of the difference between the CA78K0 and CC-RL specifications. 
Each case should be confirmed individually. |