4.4.2 Fatal errors

Table 4.4

Fatal Errors

Number

Message

Description

E0591001

Multiple input files are not allowed.

Only one input file can be specified.

Use the list file to specify multiple input files.

E0591002

The option option cannot have an argument.

An argument was specified for an option that should not have arguments.

E0591003

The option option requires an argument.

No argument was specified in an option that requires arguments.

E0591004

The option option is specified more than once.

Only one option can be specified at one time.

E0591005

Requires an output file.

The output file corresponding to the input file was not specified.

E0591006

Failed to read an input file file.

The folder name or file name may be incorrect. If the next file is specified in the list file, conversion of that file will start.

E0591007

Failed to write a result of conversion file file.

The folder name may be incorrect.

E0591008

Failed to write an output file file.

The folder name may be incorrect.

E0591009

Failed to read a list file file.

The folder name may be incorrect.

E0591010

Syntax errors in list file file.

The description of the list file is not correct.

E0591011

File name is corrupted.

There are duplicate file names among the input file, output file, and conversion result output file.

E0591012

Invalid file name.

Either the input file name specified on the command line or an input or output file name specified in the list file has exceeded 260 characters.

E0591013

Invalid argument for the option option.

The argument specification is invalid or the specified file name has exceeded 260 characters.

E0591101

Illegal syntax in string.

Conversion could not be performed because there was a syntax that is not allowed in the CA78K0R. Modify the input file.

E0591102

Can not add inline function for assembly.

The number of inline functions for assembly has exceeded the upper limit. Modify the input file.

E0591103

Failed to delete a temporary file.

Deletion of a temporary file has failed. Delete the temporary file.