r_hofc_interrupt

Performs processing in response to the timer interrupt.

Remark This API function is called as the interrupt process corresponding to the High-speed on-chip Oscillator clock Frequency Correction function interrupt INTCR.

[Syntax]

CA78K0R Compiler

__interrupt static void r_hofc_interrupt ( void );

CC-RL Compiler

static void _near r_hofc_interrupt ( void );

[Argument(s)]

None.

[Return value]

None.