r_intrtcicn_interrupt

Performs processing in response to the external maskable interrupt INTRTCICn.

Remark This API function is called as the interrupt process corresponding to the external maskable interrupt INTRTCICn.

[Syntax]

CA78K0R Compiler

__interrupt static void r_intrtcicn_interrupt ( void );

CC-RL Compiler

static void __near r_intrtcicn_interrupt ( void );

Remark n is the interrupt factor number.

[Argument(s)]

None.

[Return value]

None.