r_sg_interrupt

Performs processing in response to the threshold value detection of the logarithmic decrement interrupt INTSG.

Remark This API function is called as the interrupt process corresponding to the threshold value detection of the logarithmic decrement interrupt INTSG.

[Syntax]

CA78K0R Compiler

__interrupt static void r_sg_interrupt ( void );

CC-RL Compiler

static void __near r_sg_interrupt ( void );

[Argument(s)]

None.

[Return value]

None.