r_smotd_counterB_interrupt

Performs processing in response to the Sampling output timer compare match interrupt INTSMOTB.

Remark This API function is called as the interrupt process corresponding to the Sampling output timer compare match INTSMOTB.

[Syntax]

CA78K0R Compiler

__interrupt static void r_smotd_counterB_interrupt ( void );

CC-RL Compiler

static void __near r_smotd_counterB_interrupt ( void );

[Argument(s)]

None.

[Return value]

None.