R_TMR_RDn_ForcedOutput_Stop

Ends the pulse output forced cutoff for 16-bit timer RDn.

Remark This API function can only be called when the 16-bit timer RDn is the count to stopped (the TSTART bit in the timer RD start register (TRDSTR) is 0).

[Syntax]

void R_TMR_RDn_ForcedOutput_Stop ( void );

Remark n is the channel number.

[Argument(s)]

None.

[Return value]

None.