r_uartmgn_callback_error

Performs processing in response to the UARTMG reception error interrupt INTSREMGn.

Remark This API function is called as the callback routine of interrupt process r_uartmgn_interrupt_error corresponding to the UARTMG reception error interrupt INTSREMGn.

[Syntax]

#include r_cg_macrodriver.h

static void r_uartmgn_callback_error ( uint8_t err_type );

Remark n is the channel number.

[Argument(s)]

I/O

Argument

Description

O

uint8_t err_type;

Trigger for UART reception error interrupt

00000xx1B: Overrn error

00000x1xB: Framing error

000001xxB: Parity error

[Return value]

None.