Usage example

Measure temperature by measuring the output voltage from the temperature sensor using the A/D converter.

[GUI setting example]

Temparature sensor

Used

TS

Used

Temparature sensor operation setting

Used

Operation mode setting

Normal-temparature range (mode 2)

A/Dconvertor

Used

ADC

Used

A/D convertor operation setting

Used

Comparator operation setting

Stop

Resolution setting

8 bits

VREF(+) setting

Internal reference voltage

VREF(-) setting

VSS

Trigger mode setting

Software trigger mode

Operation mode setting

On-shot select mode

ANI0 - ANI5Analog input selection

All digital

A/D channel selection

Temparature sensor output voltage

Conversion time mode

Normal 1

Conversion time

544/fCLK 22.6667(μs)

Conversion result upper/lower bound value setting

Generates an interrupt request (INTAD) when ADLL≦ADCRH≦ADUL

Upper bound (ADUL) value

255

Lower bound (ADLL) value

0

Use A/D interrupt (INTAD)

Used

Priority

Low

[API setting example]

r_cg_main.c

void main(void)

{

R_MAIN_UserInit();

/* Start user code. Do not edit comment generated here */

/* Start the temperature sensor operation */

R_TMPS_Start();

/* Start the AD converter */

R_ADC_Start();

while (1U)

{

;

}

/* End user code. Do not edit comment generated here */

}

r_cg_adc_user.c

/* Start user code for global. Do not edit comment generated here */

volatile uint8_t g_adc_value;

/* End user code. Do not edit comment generated here */

static void __near r_adc_interrupt(void)

{

/* Start user code. Do not edit comment generated here */

/* Stop the AD converter */

R_ADC_Stop();

/* Return the higher 8 bits conversion result */

R_ADC_Get_Result_8bit((uint8_t *)&g_adc_value);

/* End user code. Do not edit comment generated here */

}